Title

Spróbuj wyszukać według słowa kluczowego, kodu zamówieniowego, kodu produktu lub numeru seryjnego np. "CM442" lub "Karta katalogowa"
Aby rozpocząć wyszukiwanie, należy wprowadzić minimum 2 znaki.

From the laboratory to the field with Raman spectroscopy

Evonik's scalable PAT solution – for greater efficiency, safety, and quality in specialty chemicals manufacturing

Przemysł: Przemysł chemiczny
Process Engineer and Endress+Hauser Raman probe at Evonik

Podsumowanie

In partnership with Endress+Hauser, Evonik has successfully integrated Raman spectroscopy as a powerful process analysis technology (PAT) from the laboratory to pilot plants, right through to production. This technology delivers real-time data, increases efficiency, reduces costs, and improves product quality. Its flexibility, scalability, and safety make it the key to new savings potential in chemical process development. Customers can benefit directly from this acquired expertise to optimize their own development and production processes in a sustainable manner.

The results: Greater efficiency, safety, and quality

16

installed Raman Rxn2 analyzers

50+

measuring points with Raman Rxn probes

Raman spectroscopy from Endress+Hauser has established itself as a key PAT tool at Evonik. It enables significant efficiency gains, cost reductions, and faster market launch of new products.

Results include:

  • End-to-end process analysis from the laboratory to production
  • Real-time measurements possible at several measuring points at the same time
  • Inline measurements replace manual sampling
  • Suitability for pilot plants with low volumes
  • Reliable operation even under difficult conditions (e.g., ATEX zones)
  • Reduction in the time to market
  • Cost reduction through elimination of laboratory evaluations and reduced personnel costs
  • Increased safety
  • Internal acceptance and acquisition of expertise
Photo of Dr. Andreas Ohligschläger, PAT Engineer, Evonik Industries AG

"With Raman spectra, you might be able to assign isolated peaks to individual substances in the mixture. This significantly reduces the calibration effort and quickly leads to quantitative results."

Dr. Andreas Ohligschläger, PAT Engineer, Evonik Industries AG

The challenge: Find a versatile, real-time lab-to-process solution

Back in 2016, Evonik launched its company-wide “lab to process” strategy with the aim of embedding PAT technologies early on in process development. Evonik was looking for a process analysis technology that would efficiently support the entire development and optimization process while also helping to reduce costs. The goal was to find a solution that not only provides accurate real-time data but is also versatile enough to be used in a wide variety of process environments – from the laboratory to production.

The technology should:

  • be universally applicable for a wide range of chemicals, states of matter and process conditions
  • be flexible and scalable from the R&D lab to large-scale production facilities
  • be quick to integrate in order to shorten development times and reduce time to market
  • improve product quality through continuous inline measurements
  • function reliably even under demanding conditions such as ATEX zones

Our solution: A scalable PAT Endress+Hauser Raman spectroscopy system

Endress+Hauser provided Evonik with a customized solution based on Raman spectroscopy – a technology that meets all of the requirements outlined. The systems are characterized by their exceptional modularity and versatility. Thanks to optical fibers and various probe types, they can be easily integrated into a wide variety of installation situations. Up to four independent channels enable simultaneous monitoring of multiple measuring points – a clear advantage for complex processes.

The chemometric suitability of the spectra offers particular added value – due to compatibility with all common chemometric programs, these can be analyzed directly on the spectrometer in a way that is versatile, intuitive, and achieved in real time. This allows qualitative and quantitative data to be recorded and interpreted immediately during the process – without any time-consuming manual sampling.

Raman spectroscopy was successfully used for the first time in a pilot plant for the development of hydrogenation processes. The probe was integrated into a 6 mm pipe – significantly smaller than in production facilities. Instead of daily NMR sampling, the technology now enables inline measurements to be taken every single minute, and the process continuously monitored.

This process is efficient, precise, and safe. In pilot plants with low volumes in particular, the system composition remains unchanged because no samples need to be taken. This not only saves time and money but also increases safety for both personnel and plant.

Hazardous area use

Thanks to its standardized and certified components, the Raman system can even be used in ATEX zones at a cost that is reasonable. For use in potentially explosive atmospheres, Evonik also uses the Liquiphant Vibronic level switch. This ensures that no flammable gas mixture can form in the laser beam of the Raman probe – a decisive contribution to process safety.

Testimonial

Photo of Dr. Roland Peschke, PAT expert at specialty chemical manufacturer Evonik

“The requirements for PAT measurement systems are particularly high, especially in the harsh environment of process plants and the need to comply with ATEX regulations. Raman spectroscopy has established itself as a robust and reliable tool in this area.” - Dr. Roland Peschke, PAT expert at Evonik Oxeno

Global roll out

This system has enabled Evonik not only to increase efficiency and quality in process development, but also to successfully transfer technology from the laboratory to production – a real key to new savings potential. Following successful implementation in Germany, Raman technology is now being rolled out internationally in Evonik’s first production plants – supported by the global expertise of Endress+Hauser.

Free download

Download the case study

Want access to the full case study as a PDF? Download a copy to read at your convenience, save for future reference, or share with colleagues.

Download the case study

Skontaktuj się z nami

Czy jesteś zainteresowany naszą ofertą? Czy chciałbyś porozmawiać o swojej aplikacji?

Prosimy o jak najbardziej szczegółowe informacje, jak możemy Ci pomóc. Dzięki temu będziemy mogli udzielić Ci najlepszej możliwej odpowiedzi.

Products and services used

/

Related solutions and technology

Analiza optyczna

Optyczne systemy analityczne do monitorowania składu i stężenia w ciałach stałych, cieczach, zawiesinach, cząstkach i gazach – do zastosowań laboratoryjnych, procesowych oraz do monitorowania emisji.

Więcej informacji

Monitoring of effluent discharge 

Operate wastewater discharge within legal limits with complete, reliable monitoring for continuous values and fast response to contamination.

Read more

Hydrogen measurement in natural gas pipelines

Fast, continuous hydrogen measurement in natural gas pipelines enables safe blending, quality compliance and dynamic control using Raman spectroscopy - without consumables or flaring

Read more

Biomethane quality analysis for safe and compliant gas injection 

Ensure reliable biomethane quality with fast, accurate online measurement of H₂S, water dew point and critical parameters for safe grid injection and efficient operations. 

Read more

Protect reverse osmosis membranes with online water quality monitoring for desalination 

Reliable online water quality monitoring to protect RO (Reverse Osmosis) membranes, reduce cleaning effort, and extend membrane lifetime in desalination and water reuse applications

Read more

Wykrywanie nieszczelności w zbiornikach kriogenicznych (LNG, etylen, LPG i amoniak)

Wykrywanie wycieków ze zbiorników kriogenicznych na wczesnym etapie pozwala zachować kontrolę nad sytuacją. Endress+Hauser zapewnia ciągłe, niezawodne monitorowanie temperatury, chroniąc ludzi, urządzenia oraz infrastrukturę krytyczną.

Więcej informacji

Pomiar i weryfikacja CCUS w czasie rzeczywistym

Odkryj przyszłość rozwiązań w zakresie wychwytywania dwutlenku węgla: precyzyjnego, niezawodnego i dostosowanego do zastosowań w fazie gęstej

Więcej informacji

Rozwiązania do ciągłego monitorowania emisji zapewniające zgodność z przepisami

Rozwiązania do ciągłego monitorowania emisji zapewniające zgodność z przepisami

Więcej informacji

FAQs

Company logo of: Evonik Industries AG

Evonik Industries AG z siedzibą w Essen, w Niemczech, to światowy lider w branży specjalistycznych produktów chemicznych. Dzięki pasji do innowacji i doskonałości technicznej firma przekracza granice tradycyjnej chemii, tworząc zrównoważone rozwiązania dla przemysłu i społeczeństwa. Evonik zarządza zakładami produkcyjnymi w 27 krajach na sześciu kontynentach.