Title

Spróbuj wyszukać według słowa kluczowego, kodu zamówieniowego, kodu produktu lub numeru seryjnego np. "CM442" lub "Karta katalogowa"
Aby rozpocząć wyszukiwanie, należy wprowadzić minimum 2 znaki.

Conductivity measurement inside a flowmeter: additional process information without an extra sensor

Detect product transitions, contamination risks and cleaning phases earlier with simultaneous measurement of flow and conductivity in one sensor

Proline Promag H electromagnetic flow meters in food and beverage measuring conductivity in brewery

In many food and beverage, life sciences, chemical, water and wastewater processes, flow measurement alone does not provide enough information to understand what is happening in the pipe. Additional information is needed to determine whether the fluid is changing, whether product and cleaning phases are clearly separated, whether concentration levels remain stable or whether process conditions are beginning to deviate.

Traditionally, this often requires a separate conductivity sensor and additional process connections, increasing installation effort and maintenance requirements. In compact skids, hygienic processes or retrofit projects, every additional sensor can also increase complexity and potential cleaning or leakage risks.

Conductivity measurement with Promag or Picomag flowmeters helps address this challenge by combining electromagnetic flow measurement and conductivity information in one measuring point.

Integrated conductivity measurement at a glance
  • What is integrated conductivity measurement with Promag/Picomag? Integrated conductivity measurement with Promag/Picomag means that the electromagnetic flowmeter measures not only flow, but also the electrical conductivity of the process medium using the existing measuring electrodes.
  • What problem does it solve? It provides additional process information without a separate conductivity sensor, reducing extra process connections, installation effort and maintenance requirements.
  • What are the key benefits? Conductivity measurement with our electromagnetic flowmeters helps provide additional process transparency, supports media identification, enables phase separation in cleaning processes, reduces the need for additional measuring points and can lower installation and maintenance effort.
  • When should it be used? It is particularly valuable when conductivity is needed as a process signal, for example to detect product changeovers, control CIP and SIP phases, monitor concentration, detect contamination or unwanted media ingress, support quality checks or identify changes in water and wastewater processes.

Why conductivity is an important process indicator

Electrical conductivity describes how well a liquid conducts electrical current. It depends mainly on the ion concentration in the medium and on temperature. Because different liquids and concentrations often have different conductivity values, conductivity can be used as a practical indicator for process and media changes.

In daily operation, conductivity information can help identify product-to-water transitions, distinguish cleaning media from product, monitor concentration changes, support quality control and detect deviations in the process. It can also reveal unwanted impurities or contamination – for example due to the ingress of water, cleaning agents or foreign media into the product – because even small amounts of an intruding substance can noticeably change the conductivity of the liquid.

For this reason, conductivity is more than an additional measured value. It is a useful process signal that supports earlier detection of deviations, reduces uncertainty and enables more informed process decisions.

conductivity measurement graphic ©Endress+Hauser

How integrated conductivity measurement within electromagnetic flowmeters works

Proline Promag and Picomag flowmeters use the electromagnetic measuring principle to determine volumetric flow. At the same time, the majority of them can also determine the conductivity of the medium using a conductive measuring method based on the existing electrodes.

As a result, one measuring point can provide two relevant process values: flow and conductivity. Compared with a separate conductivity sensor, this approach reduces additional hardware, process connections and maintenance effort while supporting a compact and transparent measurement setup.

Calibration rig for flow and conductivity measurement ©Endress+Hauser

Calibrated conductivity for greater measurement transparency

For selected Promag devices, even calibrated conductivity is available as an option. As standard, the conductivity measurement is specified with an accuracy of ±10% within the measuring range. With the calibrated conductivity option, the measurement is checked and documented during factory calibration and supplied with a calibration certificate, improving the specified accuracy to ±5%. In both cases, the measurement achieves a repeatability of up to ±1% and covers a wide measuring range from approximately 5 to 100 000 µS/cm, so it can be applied across low-conductivity water as well as higher-conductivity process media. The achievable accuracy, measuring range and response time depend on the sensor, transmitter and nominal diameter (DN) of the device.

Calibrated conductivity provides documented conductivity measurement performance and supports traceable measurement quality. This can be especially valuable when conductivity values are used for media identification, quality checks, cleaning control or documented process monitoring. Factory recalibration is also possible when a renewed confirmation of the conductivity measurement is required.

Temperature-compensated conductivity measurement

Conductivity values are temperature-dependent. If the temperature of the medium changes, the measured conductivity value changes as well. Temperature compensation helps make conductivity values more comparable and supports consistent interpretation of process conditions.
Promag H and Picomag devices with integrated temperature measurement can provide temperature-compensated conductivity directly. For Promag P and Promag W, temperature information can be supplied via analog or digital input signals and used for conductivity compensation based on a linear temperature coefficient.

Typical applications for conductivity measurement with Proline Promag and Picomag flowmeters

  • Food and beverage processes: Conductivity measurement helps reliably detect product changeovers, distinguish product and water phases and monitor CIP and SIP processes, reducing product loss and supporting efficient cleaning procedures.
  • Life sciences applications: Conductivity measurement supports media identification, cleaning verification and process monitoring in hygienic and regulated environments, helping ensure consistent production conditions.
  • Chemical processes: Conductivity measurement enables concentration monitoring and early detection of process deviations, providing valuable information for stable and efficient chemical production.
  • Water and wastewater applications: Conductivity measurement provides continuous insight into water quality and treatment processes, helps detect contamination or unexpected changes in the medium and react quickly to process variations.
  • Mining, minerals and metals processes: Conductivity measurement supports process water monitoring, concentration control in leaching as well as hydrometallurgy and early detection of process changes, helping keep operations stable and efficient.

Frequently asked questions about conductivity measurement

Find the right electromagnetic flowmeter and turn flow measurement into process insight

Whether you want to identify product transitions, improve cleaning procedures, monitor concentration or detect contamination risks, integrated conductivity measurement provides visibility beyond flow measurement.

Explore the Promag portfolio and find the right conductivity-enabled flowmeter for your application.

/