Teqwave H replaces manual refractometer measurement at Kreuzberg Quelle
Kreuzberg Quelle wanted to automate the monitoring of the sugar/invert sugar content in the soft drink filling process and was looking for an inline measuring device. Endress+Hauser offers the ideal solution with the concentration meter Teqwave H. Its state-of-the-art calculation methods enable compensation for cross-influences on a product-specific basis. This enables determining the sugar content of a wide variety of non-alcoholic beverages very accurately in the process.
Teqwave H monitors sugar concentration directly in the filling process
The transmitter of Teqwave H enables easy switching of recipes before a product change – directly in the plant or via laptop
The results
Continuous measurement of the sugar concentration in soft drinks without time-consuming manual sample measurement
Increased measuring accuracy thanks to product-specific recipes that allow compensation for cross-influences
Simplified documentation by calling up internally stored measured data
Enhanced flexibility by reading out measured values and adjusting the recipes thanks to the digital communication protocol (Modbus TCP)
Robust hygienic design and very simple in-line cleaning of the sensor
Teqwave H of Endress+Hauser is a major relief to us with its continuous and automatic monitoring of the sugar concentration. I appreciate the accuracy and reliability of the concentration measurement.
Jürgen Ackermann, Managing Director
Kreuzberg Quelle Ackermann GmbH
The challenge
Kreuzberg Quelle had previously used a handheld refractometer to monitor the Brix content during the filling process to ensure consistent quality of their soft drinks. Measuring samples of each batch manually was time-consuming and fluctuations were discovered late in the process. Therefore, they were looking for a concentration meter that monitors the Brix content continuously and eliminates the effect of cross-influences. They also wanted to monitor the measured values from various places.
Our solution
The concentration meter Teqwave H continuously measures the sugar content in various soft drinks in real time. With configurable product-specific recipes the customer can compensate for existing cross-influences (acid, CO2) and thus boost the measuring accuracy. Measured values can be read out anytime and anywhere thanks to digital communication. Deviation from set point as well as large fluctuations in the measured values can be identified quickly and product quality is ensured.
Device used
Teqwave H with “Softdrink” concentration app for measuring the sugar concentration and creating product-specific recipes for soft drinks with different acid and CO2 content
Teqwave Viewer operating software for reading out stored data
Woda, gaz ziemny, para wodna, olej mineralny i chemikalia to tylko niektóre media, których przepływ wymaga codziennych pomiarów. Dowiedz się więcej o pomiarach przepływu i wybierz przepływomierz najlepiej dostosowany do swoich potrzeb.
Każdego dnia woda, napoje, produkty mleczne, środki chemiczne i leki są poddawane analizie. Spośród kompleksowej oferty naszych produktów wybierz urządzenie najlepiej dostosowane do potrzeb Twojego procesu.
Twój partner, dzięki któremu spełnisz normy bezpieczeństwa żywności, zapewnisz stałą jakość produktów, zwiększysz moce produkcyjne oraz realizujesz inicjatywy w zakresie zrównoważonego rozwoju – nawet przy ograniczonym budżecie.
Kreuzberg Quelle Ackermann GmbH & Co. KG, Germany
Kreuzberg Quelle Ackermann has been producing over 20 different non-alcoholic beverages since 1971. These include a variety of sodas, tea beverages, fruit juices, mineral waters and spritzers, all produced with water sourced from the Kreuzbergquelle. The soft drink producer, headquartered in Hallerndorf in Germany’s Upper Franconia region, is also active as a contract bottling company.
Szanujemy Państwa prywatność
Używamy plików cookie, aby poprawić komfort przeglądania, gromadzić dane statystyczne w celu optymalnego działania witryny i wyświetlać spersonalizowane reklamy lub treści.
Wybierając "Akceptuj wszystko", wyrażacie Państwo zgodę na używanie plików cookie.
Aby uzyskać więcej informacji, prosimy o zapoznanie się z naszą Polityką plików cookie .