Spróbuj wyszukać według słowa kluczowego, kodu zamówieniowego, kodu produktu lub numeru seryjnego np. "CM442" lub "Karta katalogowa"
Aby rozpocząć wyszukiwanie, należy wprowadzić minimum 2 znaki.

Beer quality control for master brewers & breweries

Ensure stable beer quality 365 days a year with inline process instruments that monitors critical parameters in real time through the entire brewing process - from brewhouse to bottle

Brewhouse vessels equipped with Endress+Hauser inline sensors for total beer quality control

Prosimy o jak najbardziej szczegółowe informacje, jak możemy Ci pomóc. Dzięki temu będziemy mogli udzielić Ci najlepszej możliwej odpowiedzi.

Consistent beer quality through precise, real-time process monitoring

Beer is brewed from natural raw materials that change with every harvest, affecting extract yield, fermentation behavior and overall process stability. Even experienced brewers face variability that cannot be corrected by intuition alone.

To hit the same flavor profile batch after batch, breweries rely on precise inline measurements - e.g., density, flow, temperature, dissolved oxygen - to provide stable, real-time inputs for process control. These measurements reduce dependence on manual sampling and enable early detection of deviations that would otherwise appear only in lab results.

With reliable, repeatable data available at each critical step, breweries can react immediately to raw material fluctuations, maintain consistent quality and avoid costly rework or inefficiencies across the entire production process.

Modern brewhouse with stainless steel vessels for starch conversion and precise beer quality control ©Endress+Hauser

Mastering the brewhouse: Innovative measurement technology ensures precise extract yield and total beer quality control from the very first stage

Insights

Boost brewhouse efficiency with precise measurement for optimal starch-to-sugar conversion

The process begins with the efficient conversion of starch into fermentable sugars such as maltose. This step determines the wort gravity and therefore the potential of the final product. To monitor critical transition points reliable and accurate measurement technologies are essential, not optional.

Endress+Hauser offers a comprehensive product portfolio to refine every stage of your brewhouse operations.

  • Ensure highest reliability and accuracy with non-glass pH sensors like CPS77E with Memosens technology and retractable holders.
  • To monitor actual yield, the multi-frequency Coriolis mass flowmeter Promass Q provides temperature compensated flow, total value and totalized Brix or Plato° values even in entrained gas applications.
  • Rely on highest reliability in your mash tun level measurement using the temperature compensated Deltapilot FMB50 hydrostatic level sensor. Remote electronics make access easy.
  • Minimize raw material usage by adding liquified adjuncts and dextrose with high accuracy. The Coriolis mass flowmeter Promass F100 provides the best temperature stability and precise measurement.
Brew master installing new fermentation monitor QWX43 ©Endress+Hauser

Inline quality control: Brew master checking fermentation process real-time by using the multi-parameter device QWX43

Insights

Real-time insights for stable fermentation

In beer fermentation, yeast converts fermentable sugars from malt into ethanol, CO₂ and secondary flavor compounds. To ensure consistent beer quality, it is essential to monitor and control key parameters such as temperature, extract, fermentation rate and alcohol content throughout the fermentation process.

Hygienic RTDs with fast response times support stable and precise temperature control during fermentation. Continuous, real-time monitoring of key fermentation parameters provides high‑accuracy process data and enables reliable, reproducible control throughout the batch.

  • The hygienic modular thermometer iTHERM ModuLine TM411 provides fast and stable measurement to support precise temperature control in fermentation processes.
  • Real-time insights into fermentation process and better process control is provided by our multi-parameter device Fermentation Monitor QWX43.
Sight glass on a brewery process line showing filtered beer for clarity and quality control ©Brauerei Schützengarten

Transparent filter section allowing operators to monitor filter loading and flow conditions in real time.

Insights

Maximizing yield and clarity in filtration

A major challenge of conventional filtration is the use of diatomaceous earth (DE). Because DE is a mined material, its quality and filtration performance can vary significantly. In addition, DE is difficult to handle and dispose of. Spent DE is often classified as hazardous waste and generates large volumes of filter cake and effluent, making disposal both costly and environmentally burdensome.

Differential pressure is a standard and reliable indicator of filter loading and performance. Both conventional DP transmitters and modern electronic DP systems can provide stable, accurate measurements when installed and maintained correctly.

  • Enhance measurement stability and improve filter performance with electronic differential pressure system Deltabar FMD71 or with two hygiene pressure transmitter Cerabar PMP43
Liquiline CM44P allows the setup of complete measuring points for monitoring processes ©Endress+Hauser

Set-up and monitor measurement transmitter to ensure stable and accurate process values in production.

Insights

Improved process control through inline beer-type verification

Breweries often produce a wide variety of beer styles, which makes it challenging to maintain a clear overview of production status. Consistent tracking is essential to ensure that the correct product is routed to the filling line.

To keep production running smoothly and minimize beer loss, breweries need to identify different beer types automatically and directly inline. Dual‑channel photometers measure color absorbance according to EBC guidelines, while conductivity provides additional media differentiation. Combined, these measurements allow reliable identification of each beer type before it reaches the filling line.

Inserting a test cartridge into Endress+Hauser BioSense system for rapid beer spoilage detection. ©Endress+Hauser

Rapid molecular detection: The BioSense system brings PCR-based testing out of the lab and onto the plant floor to identify spoilage bacteria in hours rather than days.

Insights

Reducing quality risks through microbiological insights

Microbial contamination from spoilage bacteria can occur at multiple stages in the brewing process. Raw materials, process water, equipment surfaces and the beer itself are all potential sources of contamination. Therefore, testing critical points such as the fermentation tank, the bottling line or the brewing water is crucial. Traditionally, detection of spoilage bacteria has relied heavily on time-consuming laboratory testing.

However, there’s a more efficient approach: the Endress+Hauser BioSense Analysis System. This innovative system enables PCR-based detection of spoilage bacteria, microbial contamination, and even pathogens. With its compact design and simple workflow, the Device BAB00 enables for immediate on-site analysis, significantly reducing response times and ensuring swift corrective actions. This approach revolutionizes quality control in the brewing industry, enhancing both quality and efficiency.

CIP system with digital transmitters from Endress+Hauser for cleaning optimization ©Endress+Hauser

Increase CIP efficiency: Inline measurement instrumentation eliminate the guesswork in cleaning cycles, drastically reducing water and chemical waste.

Insights

Cleaning-in-place optimization: A pillar of consistent beer quality

CIP concentration is critical for food safety, but it also strongly influences detergent consumption and wastewater costs. Accurate monitoring and control of chemical usage are therefore key to achieving both hygienic compliance and cost‑efficient operation.

Highly accurate conductivity measurement ensures the exact calculation of the required concentration. Level measurement of aggressive chemicals can be solved using different options depending on tank size and user preference.

  • High‑accuracy conductivity measurement allows precise determination of CIP detergent concentration, ensuring effective cleaning while avoiding unnecessary chemical overuse.
  • Depending on tank size, configuration and operator preference, level measurement can be implemented using hydrostatic or radar technologies - both established, robust principles for corrosive media.
  • Fast temperature compensation in our conductivity transmitters improves phase separation accuracy, reducing beer losses during changeovers.

Explore further opportunities for CIP optimization to support quality and ensure resource efficiency.

"W mojej pracy jako Industry Manager staram się pomóc Państwu w zapewnieniu jakości i smaku produktów. Pracując razem, robimy wszystko, co w naszej mocy, aby jeszcze bardziej ulepszyć proces kontroli jakości."

Matthias Schützeberg, Industry Manager - branża spożywcza, Endress+Hauser Group Services AG
Solutions

Discover our related solutions

Wiodące w branży zarządzanie zapasami materiałów sypkich

Dowiedz się więcej o naszych światowej klasy rozwiązaniach do zarządzania stanami magazynowymi w przemyśle spożywczym oraz o tym, jak Endress+Hauser może pomóc Ci kontrolować je w wielu lokalizacjach jednocześnie.

Read more

Bezpieczne monitorowanie wody w procesach przemysłowych

Postaw na efektywne, proste i bezpieczne monitorowanie jakości wody w procesach przemysłowych z rozwiązaniami „pod klucz” Endress+Hauser.

Read more

System analizy pary i wody (SWAS)

Czy wiesz, jak jest najlepszy sposób aby chronić obieg wody/pary przed zanieczyszczeniem? Sprawdź nasze rozwiązania SWAS dla elektrowni i kotłów, obejmujące pełną technologię do monitorowania jakości wody.

Read more

Systemy monitoringu wody na wylocie z oczyszczalni dla każdej branży przemysłu

Dowiedz się więcej o oferowanych przez nas niezawodnych, gotowych do użytku systemach monitoringu ścieków z funkcją inteligentnej konserwacji, która pomoże Ci w spełnianiu ograniczeń wynikających z przepisów prawa i umów.

Read more

Przypisy końcowe

Related articles

Discover more interesting articles