The Endress+Hauser Group

Aktualności

Wydarzenia

Your career with Endress+Hauser

Oprogramowanie narzędziowe

Informacje kontaktowe

Sklep E-direct

Produkty E-direct: wysoka jakość, atrakcyjna cena oraz błyskawiczna dostawa 48h. Całodobowy dostęp do wyselekcjonowanej oferty możliwy poprzez platformę sklepu E-direct. Kupuj wygodnie przez Internet!

Sklep E-direct

Leading market position

Frost & Sullivan recognizes Endress+Hauser with the “Global Market Leadership Award” for electromagnetic flowmeters

With an installed base of more than 2 million instruments, Endress+Hauser is the market leader in electromagnetic flowmeters. US consulting firm Frost & Sullivan came to this conclusion after conducting extensive market and competitive research, thus honoring Endress+Hauser with the “Global Market Leadership Award”.

The company was recognized during Frost & Sullivan’s awards gala in California. “Endress+Hauser’s success is tied to a strong customer focus and a high level of innovation,” says Dr. Rajender Thusu, Frost & Sullivan Industry Analyst. The company invests heavily in research and product development in order to meet its customers’ requirements in the area of liquid flow measurements.

Frost & Sullivan highlighted the company’s close collaboration with customers. “Our aim is to help our customers run their processes in a reliable, safe, sustainable and economic manner. To do that, we work closely together with the customers from the very early stages of product design, to the operations phase and beyond,” says Dr. Bernd-Josef Schäfer, Managing Director of Endress+Hauser Flowtec, the Group’s competence center for flow measurement technology in Reinach, Switzerland.

Products and services for individual requirements

The Endress+Hauser product portfolio of electromagnetic flowmeters guarantees precise measurement of volume flow without restricting production flow rates or causing any pressure drop. The result is less downtime and increased productivity, which contributes to lower overall operational costs. “Most of our customers value the combination of state-of-the-art electromagnetic flow measurement instruments and the wide range of services that we offer,” emphasizes Bernd-Josef Schäfer.

Apart from the extensive portfolio of measurement instruments, Endress+Hauser also offers global support services that enable customers to optimize their processes over the plant’s entire life cycle, thus making the company more competitive. This includes calibration, diagnosis, repair, engineering, commissioning and maintenance services.

Leading technologies

The electromagnetic flowmeters from Endress+Hauser, which feature advanced engineering such as Heartbeat Technology, support various communications protocols, including EtherNet/IP and PROFINET, that make the information easily accessible.

Thanks to Heartbeat Technology, instruments such as the Proline flowmeter line have self-monitoring capabilities. By supplying process and instrument diagnostic notifications in line with NE 107, influences and changes can be detected and rectified before impacting the process – all while the process is running.

Kontakt

Masz pytania dotyczące nagrody dla światowego lidera rynku — Global Market Leadership Award?
Z chęcią wyślemy Ci dodatkowe materiały lub skontaktujemy z naszymi ekspertami.

  • Endress+Hauser was recognized with the Global Market Leadership Award for electromagnetic flowmeters ©Endress+Hauser

    Frost & Sullivan recognizes Endress+Hauser with the Global Market Leadership Award for electromagnetic flowmeters.

  • Endress+Hauser manufactures flow measurement technology at six locations ©Endress+Hauser

    Endress+Hauser manufactures flow measurement technology at six locations in Switzerland, France, the United States, China, India, and Brazil with state-of-the-art production logistics.

  • The new plant in Suzhou, China is designed for extremely large instruments with diameters. ©Endress+Hauser

    Endress+Hauser calibrates flowmeters around the world in accordance with the same standards. The new plant in Suzhou is designed for extremely large instruments with diameters of up to 3 meters.

Kontakt

Endress+Hauser Polska sp. z o.o.
ul. Wołowska 11 51-116 Wrocław , Polska
Tel.: +48 71 773 00 00
Faks: +48 71 773 00 60
Wyślij e-mail